functionID | name |
---|---|
0009 | Shutter actuator |
0061 | Blind actuator |
0062 | Attic window actuator |
0063 | Awning actuator |
pairingID | in/out | name | value |
---|---|---|---|
32 | in | Move sunblind up / down |
0 - up
1 - down
|
33 | in | Stops the sunblind and to step it up/down | |
35 | in | Moves the sunblinds into a specified position | position from 0 to 100 percent |
288 | out | indicate the move up/down and stop state |
0 - not moving
2 - moves up
3 - moves down
|
289 | out | Indicate the current position of the sunblinds in percentage | position from 0 to 100 percent |