Content
Prerequisites for using the free@home cloud API
The free@home local API is capable accessing the free@home system access points of end users when they are connected to the local network. For this, a few prerequisites have to be met by the end user.
End user
This API is capable of controlling a SysAP in the local network .
The end user must enable the activate local API setting in the SysAP settings of the free@home next App, found under More -> free@home Settings -> Local API.
The end user needs an ABB-free@home smart access point with version 2.6.0 or later.




To sum up, the end user/system access point requirements are:
A system access point 2.0 with at least version 2.6.0 must be available.
The free@home next App for a mobile device.
The system access point must enable the
activate local APIsetting underMore -> free@home Settings -> Local API.