AIP definition

GetAll

The user publishes the following topic to obtain getall information, while subscribing to the response to receive the completed JSON response.

Response example

Set DataPoint

Users publish the following topics to set SmartAP datapoints, while subscribing to topics to receive JSON responses.

This is an example of opening outdoor station with serial number "101807A7F04AAA0".
***Is_ Secondlock * * *=0 represents the default lock, * * * is_ Secondlock * * *=1 represents an auxiliary lock

In the example the device 101807A7F04AAA0 has one channel (ch0001) with the datapoint of "idp0000" which represents an outdoor station door opener.

value equals to 1 means door open.

Notification

Users regularly send heatbeats (30s) to maintain online status, while subscribing to the following notifications
Receive message push when SmartAP has notifications

Notification sample

In the example the device 101807A7F04AAA0 has one channel (ch0000) with the datapoint of oidp0000" which represents an outdoor station door opener status.

value equals to 1 means door status is open.