Prerequisites for using the Welcome IP local API
The welcome IP local API is capable accessing the door entry system access points of end users when they are connected to the local network. For this, a few prerequisites have to be met by the end user.
Topology

The 3rd Party Panel/APP want to use the local API function need connect to the same network as the smart AP.